JN5169 - ZBPro Stack - Reading data from end device using Coordinator.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN5169 - ZBPro Stack - Reading data from end device using Coordinator.

1,910件の閲覧回数
matthew3
Contributor III

Hi all

I am reading a value from a potentiometer through one of the ADC channels on the JN5169 for testing purposes. The potentiometer will be replaced with a sensor when i have the program doing what i need to do with it. I am wanting to packet this value up and be able to read it from the coordinator which in turn will save this to a MySQL DB.

I am struggling on finding where to place my code. I am using the JN-AN-1229-ZigbeePro-Application-Template files.

Any help is much appreciated.

regards

Matthew

ラベル(4)
タグ(2)
0 件の賞賛
返信
1 返信

1,801件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Matthew, I hope you're doing well!

 

To get an idea of how to implement a sensor or a voltage measurement, you could check the JN-AN-1220 Sensors application note. It shows the creation of the clusters and endpoints required, as well as the implementation of the report to send the information to a coordinator.

 

This example shows a few different implementations, so it should be helpful to get an idea.

 

Zigbee 3.0 Application Note software.

 

Please let me know if you have any further questions.

 

Best regards,

Sebastian

0 件の賞賛
返信