JN5169 How to change the port for LED??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5169 How to change the port for LED??

3,261 Views
choisanghyun
Contributor I

Hello sir,

I have a question.

Environment ===============

- JN-AN-1189-Zigbee-Ha-Demo code

- test code : Common_Light with DimmableLightOpenHome

   Using : DriverBulb_DR1175.c 

=========================

In above environment, I want to change the LED port for indication.

But I can not find how to change it

And I want to see the DR1175 board set code, which file do I check it?

I hope you give some advise.

Another quesiton.

================================================

- C:\NXP\bstudio_nxp\sdk\JN-SW-4168\Platform\DK4 

     DK4 folder has Build,Include,Library folder.

If I changed the include file, how to build it and how to adjust it?

=================================================

I need your help.

Thanks.

Tags (1)
0 Kudos
Reply
9 Replies

3,059 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Choi,

And I want to see the DR1175 board set code, which file do I check it?

I'm sorry, could you please look at the "C:\NXP\bstudio_nxp\sdk\JN-SW-4170\Platform\DK4\Source\LightingBoard.c".

Some LEDs are configured as Output pin and PWM.

 

If I changed the include file, how to build it and how to adjust it?

Did you change the location? You could add your h file in the project.

Regards,

Mario

0 Kudos
Reply

3,059 Views
choisanghyun
Contributor I

Hi Mario.

I used JN-SW-4168, it does not have Source directory.

Do I need to update or used another SDK?

Regards,

ChoiDirectory.png

0 Kudos
Reply

3,059 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Choi,

I'm sorry, you could try the JN-AN-1218 Light Bulb example and the Zigbee 3.0 Stack JN-SW-4170.

Sorry for any inconvenience.

Regards,

Mario

0 Kudos
Reply

3,059 Views
choisanghyun
Contributor I

Hi Mario,

Can you give me another way to use driverbulb?

============================== 

And I will try below procedure.

- Use JN-SW-4168

- example code : Common light with  DimmableLightOpenHome

- make new DriverBulb(change Dio port for my board)  

- compile and use it? 

- if you have any document for making new driverbulb, give me the link.  

=============================

Regards,

Choi

0 Kudos
Reply

3,059 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,  

The example is setting the PWM in that DIO.

Please see how the example implementation, you could use for your own driver.

PUBLIC bool_t bWhite_LED_Enable(void)
{
  /* Configure timer 0 to generate a PWM output on its output pin */
  vAHI_TimerEnable(WHITE_LED_TIMER, WHITE_LED_TIMER_PRESCALE, FALSE, FALSE, TRUE);
  vAHI_TimerConfigureOutputs(WHITE_LED_TIMER, FALSE, TRUE);
  vAHI_TimerClockSelect(WHITE_LED_TIMER, FALSE, TRUE);

  return TRUE;
}


PUBLIC bool_t bWhite_LED_On(void)
{
 vAHI_TimerStartRepeat(WHITE_LED_TIMER, gu16PwmLastValue , PWM_COUNT );
 return TRUE;
}

Hope it helps.

Regards,

Mario

0 Kudos
Reply

3,059 Views
choisanghyun
Contributor I

Hi Mario,

Your answer is very useful for me. Thank you.

And I have another quesiton.

1. Do you have a example code for GPIO/ADC/I2C/EEPROM and so on ?

   It is not easy to make code to see API. Because API just explain function prototype.

   If you have the example code, I think it will help a lot.

Best regards,

Choi

0 Kudos
Reply

3,059 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Choi,

Please look at the next applications notes that implement some examples.

JN-AN-1218 - Implements DIO and PWM.

                       Implements EEPROM, app_scenes.c PDM_eSaveRecordData

JN-AN-1220 - Implements the ADC

The I2C depends on your application.

vAHI_SiMasterConfigure(FALSE, // bPulseSuppressionEnable
        FALSE, 
        31);  Operating frequency = 16/[(PreScaler + 1) x 5] MHz


vAHI_SiMasterWriteSlaveAddr(0x69, 0/*E_AHI_SI_SLAVE_RW_SET*/); 

if(bAHI_SiMasterSetCmdReg(E_AHI_SI_START_BIT,
      E_AHI_SI_NO_STOP_BIT, 
      E_AHI_SI_NO_SLAVE_READ, 
      E_AHI_SI_SLAVE_WRITE, 
      E_AHI_SI_SEND_ACK, 
      E_AHI_SI_NO_IRQ_ACK))
{
 //TO DO
}

For a better reference please look at the JN516x Integrated Peripherals API User Guide

Regards,

Mario

0 Kudos
Reply

3,059 Views
choisanghyun
Contributor I

Hi,

Thank you for your reply. It is very useful.

I have another question.

- example code

 1. ZigBee CPU : JN5169

 2. Use JN-SW-4168, JN-AN-1189-HA-DEMO

 3. Enddevice : DimmableLightOpenHome

     Coordinator : Coordinator

In above condtion, I check the network connection but I can not understand how to opertion.

Can you explain the above example[how to operation]??  

 =====================================================

- coordinator side log :

 

[COOR]APP: vCheckStackEvent: vCheckStackEvent: ZPS_EVENT_NEW_NODE_HAS_JOINED, Nw
k Addr=0x3ab4                                 
APP: No event to process                              
[COOR]sStackEvent.eType = 1                                
[COOR]APP: vCheckStackEvent: ZPS_EVENT_AF_DATA_INDICATION
                    

      Profile : 0                         

      Cluster :13                                              

      EndPoint:0
                                                            
APP: No event to process                                          
[COOR]sStackEvent.eType = 14                                        
[COOR]APP: vCheckStackEvent: ZPS_EVENT_ROUTE_DISCOVERY_CFM        
APP: No event to process                                          
[COOR]sStackEvent.eType = 0                                   
[COOR]sStackEvent.eType = 0                           
[COOR]sStackEvent.eType = 0 

 =====================================================

- enddevice side log :

Entering cbZCL_EndpointCallback
[task] 0x1d

[task] EP EVT: Invalid evt type 0x1d
Entering cbZCL_EndpointCallback
[task] 0x1d

[task] EP EVT: Invalid evt type 0x1d
[node]POR Identify


[node] Stack Event
[zbp_uti] APP_ZPR_Light_Task event:20
[zbp_uti]Unhandled Stack Event

 [node] E_RUNNING

[node]POR Identify


[node] Stack Event
[zbp_uti] APP_ZPR_Light_Task event:20
[zbp_uti]Unhandled Stack Event

 [node] E_RUNNING
 =====================================================

Best regards,

Choi

0 Kudos
Reply

3,059 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Choi,

Could you please look at the JenOs that is implemented in the SDK that you are working on?

https://www.nxp.com/docs/en/user-guide/JN-UG-3075.pdf

Regards,

Mario

0 Kudos
Reply