JN5168 sleep mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN5168 sleep mode

1,523件の閲覧回数
29603655
Contributor I

Hello:

  I use the function vAHI_Sleep(E_AHI_SLEEP_OSCON_RAMON) to let MCU enter sleep mode, but it always enter program mode when it wakeup. I check that because I use the SPIMISO pin as button, when JN5168 wakeup and the button press at the same time it will enter program mode.

  So how to disable JN5168 wake up from boot phase.

Thanks

BR

0 件の賞賛
返信
1 返信

1,408件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Liang,

To avoid programming mode: leave pin floating high during reset to avoid entering UART. 

If that specific pin is used for a button, you could try to connect to high.

Please let me know your findings.

Regards,

Mario

0 件の賞賛
返信