JN5168 UART only receive 5 bytes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN5168 UART only receive 5 bytes

2,360件の閲覧回数
29603655
Contributor I

I only can receive 5 bytes from UART0 with JN5168. Who can tell what the reason is? Thank you!

void UartInit(void)
{
    vAHI_UartSetRTSCTS(UART, FALSE);
    vAHI_UartEnable(UART);

    /* Reset UART */
    vAHI_UartReset(UART, TRUE, TRUE);
    vAHI_UartReset(UART, FALSE, FALSE);

    vAHI_UartSetBaudRate(UART, E_AHI_UART_RATE_115200);

    /* Set remaining settings */
    vAHI_UartSetControl(UART, FALSE, FALSE, E_AHI_UART_WORD_LEN_8, TRUE, FALSE);
    vAHI_UartSetInterrupt(UART, FALSE, FALSE, TRUE, TRUE, E_AHI_UART_FIFO_LEVEL_1);

    vInitPrintf((void *)vPutChar);
}

PRIVATE void vProcessIncomingHwEvent(AppQApiHwInd_s *psAHI_Ind)
{
    if (psAHI_Ind->u32DeviceId == E_AHI_DEVICE_UART0)
    {
        if ((psAHI_Ind->u32ItemBitmap & 0x000000FF) == E_AHI_UART_INT_RXDATA)
        {
            /* Store Data */
            uart0_rxBuffer[uart0_rd] = (uint8)((psAHI_Ind->u32ItemBitmap & 0x0000FF00) >> 8);
            uart0_rd = (uart0_rd + 1) % RX_BUFF_SIZE;
        }
    }
}

0 件の賞賛
返信
3 返答(返信)

2,220件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Liang Guo,

You are enabling the interrupt. You could use the ISR.

PUBLIC void APP_isrUart(void)
{
    unsigned int irq = ((*((volatile uint32 *)(UART_START_ADR + 0x08))) >> 1) & 0x0007;
    uint8 u8Byte;

    if (irq & E_AHI_UART_INT_RXDATA) {
        uint8 u8Byte = u8AHI_UartReadData(UART);
        if(ZQ_bQueueSend(&APP_msgSerialRx, &u8Byte) == FALSE)
        {
            /* Failed to send the message to queue */
        }
    }

    if (irq & E_AHI_UART_INT_TX) {
        if(ZQ_bQueueReceive(&APP_msgSerialTx, &u8Byte) == TRUE)
        {
            vAHI_UartWriteData(UART, u8Byte);
            /* decrement activity counter for dequeued data */
        } else {
            /* disable tx interrupt as nothing to send */
            UART_vSetTxInterrupt(FALSE);
        }
    }
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Mario

0 件の賞賛
返信

2,220件の閲覧回数
29603655
Contributor I

Hi Mario:

   Thank you for your reply!I use the ISR but it can't work, so I can only use the APP Queue API.

0 件の賞賛
返信

2,220件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Liang Guo,

Did you solver the uart callback?

Regards,

Mario

0 件の賞賛
返信