JN5168 I2C Communication Example Code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5168 I2C Communication Example Code

3,984 Views
xview
Contributor I


Dear Friends,

Does anyone have I2C  example code of  JN5168? I used JN5168 connecting to a MMA8451Q accelerometer sensor, but it response nothing.  Thank you.

Xview

Labels (1)
0 Kudos
Reply
4 Replies

3,003 Views
dheerajsawant
Contributor V

Hello Sir, 

i have attached photo copy. in that APPmainloop() says in non control mode program executes repedately and in control mode it will execute only one time. 

and this main loop restart after 20 sec i don't understand  how to stop this. 

My I2C is not working because of this.. 

i am checking pulses its showing as per protocol but output is not showing proper. please need help

 prmainloop.png

i think restart is my issue.

please suggest related to this problem..

thank You for your time!

0 Kudos
Reply

3,003 Views
alfredochoperen
Contributor I

The following is used with a RTC chip.  Feel free to adapt.:

/****************************************************************************

*

* NAME: vI2C_Read

*

* DESCRIPTION: I2C read function

*

* PARAMETERS: Name            RW  Usage

* u8 Address R Address of desired byte in the RTC

* pau8ReadBuffer R pointer to data buffer

* ui8Length R number of bytes to read

*

* RETURNS: Nothing

* None.

*

* NOTES:

* None.

****************************************************************************/

PUBLIC uint8 vI2C_Read(uint8 u8SlaveAddress, uint8 u8RegisterAddress,

  uint8 *u8ReadBuffer, uint8 ui8Length)

{

    uint8 i=0;

// DBG_vPrintf(TRACE_I2C, "I2C_Read::Start - I2C: %x, Reg: %d, Len: %d\n",

// u8SlaveAddress, u8RegisterAddress, ui8Length);

   // set slave address

  vAHI_SiMasterWriteSlaveAddr(u8SlaveAddress >> 1, FALSE);

  vAHI_SiMasterSetCmdReg(E_AHI_SI_START_BIT,

  E_AHI_SI_NO_STOP_BIT,

  E_AHI_SI_NO_SLAVE_READ,

  E_AHI_SI_SLAVE_WRITE,

     E_AHI_SI_SEND_ACK,

     E_AHI_SI_NO_IRQ_ACK);

  while(bAHI_SiMasterPollTransferInProgress()); // wait while busy

// DBG_vPrintf(TRACE_I2C, "I2C_Read:: Setting register address\n");

  vAHI_SiMasterWriteData8(u8RegisterAddress); // RTC address to read from

  vAHI_SiMasterSetCmdReg(E_AHI_SI_NO_START_BIT,

  E_AHI_SI_NO_STOP_BIT,

  E_AHI_SI_NO_SLAVE_READ,

  E_AHI_SI_SLAVE_WRITE,

  E_AHI_SI_SEND_ACK,

  E_AHI_SI_NO_IRQ_ACK);

  while(bAHI_SiMasterPollTransferInProgress()); // wait while busy

    /* check to see if we get an ACK back*/

    if(bAHI_SiMasterCheckRxNack())

    {

        return (1);

    }

    /* check to see if anyone else has taken the bus */

    if(bAHI_SiMasterPollArbitrationLost())

    {

        return (2);

    }

  vAHI_SiMasterWriteSlaveAddr(u8SlaveAddress >> 1,TRUE);

  vAHI_SiMasterSetCmdReg(E_AHI_SI_START_BIT,

  E_AHI_SI_NO_STOP_BIT,

  E_AHI_SI_NO_SLAVE_READ,

  E_AHI_SI_SLAVE_WRITE,

  E_AHI_SI_SEND_ACK,

  E_AHI_SI_NO_IRQ_ACK);

  while(bAHI_SiMasterPollTransferInProgress()); // wait while busy

// DBG_vPrintf(TRACE_I2C, "I2C_Read:: Reading data\n");

// now we read data from the RTC

    while(ui8Length > 0x00)

    {

        if(ui8Length < 0x02)    /* is it the last byte */

        {

        vAHI_SiMasterSetCmdReg(E_AHI_SI_NO_START_BIT,

        E_AHI_SI_STOP_BIT,

        E_AHI_SI_SLAVE_READ,

        E_AHI_SI_NO_SLAVE_WRITE,

        E_AHI_SI_SEND_NACK,

        E_AHI_SI_NO_IRQ_ACK);

        }

        else

        {

            vAHI_SiMasterSetCmdReg(E_AHI_SI_NO_START_BIT,

                E_AHI_SI_NO_STOP_BIT,

                E_AHI_SI_SLAVE_READ,

                E_AHI_SI_NO_SLAVE_WRITE,

                E_AHI_SI_SEND_ACK,

                E_AHI_SI_NO_IRQ_ACK);

        }

    while(bAHI_SiMasterPollTransferInProgress()); // wait while busy

        u8ReadBuffer[i++] = u8AHI_SiMasterReadData8();

        ui8Length--;

    }

  return (0);

}

/****************************************************************************

*

* NAME: vI2C_Write

*

* DESCRIPTION:

*

* PARAMETERS:      Name            RW  Usage

* None.

*

* RETURNS:

* None.

*

* NOTES:

* None.

****************************************************************************/

PUBLIC uint8 vI2C_Write(uint8 u8SlaveAddress, uint8 u8RegisterAddress,

  uint8 *u8WriteBuffer, uint8 ui8Length)

{

    uint8 i=0;

    // set slave address

  vAHI_SiMasterWriteSlaveAddr(u8SlaveAddress >> 1,FALSE);

  vAHI_SiMasterSetCmdReg(E_AHI_SI_START_BIT,

  E_AHI_SI_NO_STOP_BIT,

  E_AHI_SI_NO_SLAVE_READ,

  E_AHI_SI_SLAVE_WRITE,

  E_AHI_SI_SEND_ACK,

  E_AHI_SI_NO_IRQ_ACK);

  while(bAHI_SiMasterPollTransferInProgress()); // wait while busy

    /* check to see if we get an ACK back*/

    if(bAHI_SiMasterCheckRxNack())

    {

    return (1);

    }

    /* check to see if anyone else has taken the bus */

    if(bAHI_SiMasterPollArbitrationLost())

    {

    return (2);

    }

  vAHI_SiMasterWriteData8(u8RegisterAddress); // address to write

  vAHI_SiMasterSetCmdReg(E_AHI_SI_NO_START_BIT,

  E_AHI_SI_NO_STOP_BIT,

  E_AHI_SI_NO_SLAVE_READ,

  E_AHI_SI_SLAVE_WRITE,

  E_AHI_SI_SEND_ACK,

  E_AHI_SI_NO_IRQ_ACK);

  while(bAHI_SiMasterPollTransferInProgress()); // wait while busy

    /* check to see if we get an ACK back*/

    if(bAHI_SiMasterCheckRxNack())

    {

    return (3);

    }

    /* check to see if anyone else has taken the bus */

    if(bAHI_SiMasterPollArbitrationLost())

    {

    return (4);

    }

   // now we write data to the RTC

    while(ui8Length > 0x00)

    {

        /* data to write */

        vAHI_SiWriteData8(u8WriteBuffer[i++]);

        if(ui8Length < 2)    /* is it the last byte */

        {

             vAHI_SiMasterSetCmdReg(E_AHI_SI_NO_START_BIT,

                             E_AHI_SI_STOP_BIT,

                             E_AHI_SI_NO_SLAVE_READ,

                             E_AHI_SI_SLAVE_WRITE,

                             E_AHI_SI_SEND_NACK,

                             E_AHI_SI_NO_IRQ_ACK);

        }

        else

        {

            vAHI_SiMasterSetCmdReg(E_AHI_SI_NO_START_BIT,

                             E_AHI_SI_NO_STOP_BIT,

                             E_AHI_SI_NO_SLAVE_READ,

                             E_AHI_SI_SLAVE_WRITE,

                             E_AHI_SI_SEND_ACK,

                             E_AHI_SI_NO_IRQ_ACK);

        }

        ui8Length--;

        while(bAHI_SiMasterPollTransferInProgress()); /* wait while busy */

        /* check to see if we get an ACK back*/

        if(bAHI_SiMasterCheckRxNack())

        {

        return(5);

        }

        /* check to see if anyone else has taken the bus */

        if(bAHI_SiMasterPollArbitrationLost())

        {

            return(6);

        }

    }

    return (0);

}

0 Kudos
Reply

3,003 Views
dheerajsawant
Contributor V

Hello davidashrafdereksnell‌,

I AM stuck at a point.. 

i am using JN-AN-1162 application note. 

in that i am using DeviceRemote.c file

in that main loop is present  but that main loop restart after 20sec my i2c is not working because of that. 

i am interfacing JN5168 with SHT31-DIS-B. its showing me output but not showing proper Heater Enable and Disable status 

please help...

Thank you for your time

0 Kudos
Reply

3,003 Views
dheerajsawant
Contributor V

Hello @Alfredo Choperena,

i am little bit familiar with JN5168 codes. i am going by step by step to achieve main goal.

i worked with DIO,ADC,TickTimer.

right now i am working with I2C.

I am stuck in I2C communication of JN5168 with SHT31 -DIS-B.

Need Your suggestion. 

Thank You For your Time!

0 Kudos
Reply