[JN1569] Switch External crystal OSC to Internal OSC FAIL?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[JN1569] Switch External crystal OSC to Internal OSC FAIL?

ソリューションへジャンプ
4,932件の閲覧回数
manhnc
Contributor I

Hi ,

I'm beginner of JN1569 NXP chip.

I'm have test flow:

1. JN1569 startup with external crystal oscillator => it work OK.

2. pull Down 1 pin of external crystal => device fail and I wait it restart with internal oscillator BUT it don't restart.

My question:

1. JN1569 default start with internal or external OSC? And can I configure it? What is the document descript it?

2. When JN1569 working with external crytal OSC, external OSC fail, can it switch to internal OSC? If it can, how can I configure it?

Can you help me @mario_castaneda 

Thanks a lot for your help,

 

0 件の賞賛
返信
1 解決策
4,878件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @manhnc,

This condition is called a stack overflow and results in the processor stack corrupting the heap (and potentially the application).

Please look at the vAHI_SetStackOverflow function that describes this scenario.

JN516x Integrated Peripherals API User Guide

Regards,

Mario

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
4,892件の閲覧回数
manhnc
Contributor I

Hi @mario_castaneda ,

Thanks for your reply. 

I will read and check again.

And I have others question:

What happens when nxp JN1569 "Ram usage full"?

1. watchdog Reset?

OR

2. Hard fault? and where is Hard Fault handler in code (I use BeyoundStudio and skd  JN-SW-4170).

What is the document descript it?

Thanks for your help.

0 件の賞賛
返信
4,879件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @manhnc,

This condition is called a stack overflow and results in the processor stack corrupting the heap (and potentially the application).

Please look at the vAHI_SetStackOverflow function that describes this scenario.

JN516x Integrated Peripherals API User Guide

Regards,

Mario

0 件の賞賛
返信
4,862件の閲覧回数
manhnc
Contributor I

Hi @mario_castaneda ,

Thank you so much, I will implement and test it.

And I have others question: 

>> Is there any hardware failure ("hard fault") in the JN5169 chip? And where I can handle it?

Scenario, when my device real work, some device suspended (can't restart again). It works again only I power off reset it. I think it can be "hard fault" when restart (please view my image).   

Thank you,

jn5169.png

0 件の賞賛
返信
4,819件の閲覧回数
manhnc
Contributor I

Hi @mario_castaneda ,

I find more Exception in file name "AppBuildExceptionHandlers.ld". (attach file).

1. But, I don't know what exception name handle "Hard fault"? what does document descript all exception?

 2. How can I work with this file ("*.ld")?

Thank you should much!

Manhnc

 
 

 

 

 

 

 

 

0 件の賞賛
返信
4,798件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @manhnc,

Please look at the datasheet, you will find the information regarding the specific issue that you are facing.

9.5 Interrupt system https://www.nxp.com/docs/en/data-sheet/JN5169.pdf

Regards,

Mario

0 件の賞賛
返信
4,777件の閲覧回数
manhnc
Contributor I

Thanks @mario_castaneda,

It useful for me. Now, I ready clear about it. 

Further, I also have question:

Is this configuration (attach image) will make MCU restart (cold startup) when it occur?

ExceptionFile (3).PNG

0 件の賞賛
返信
4,898件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @manhnc,

The crystal oscillator is driven from an external 32kHz crystal connected to DIO9 and DIO10. If used, the external clock module is connected to DIO9.

1. JN1569 default start with internal or external OSC? And can I configure it? What is the document descript it?

JN516x Integrated Peripherals API User Guide 

The default clock source is the internal 32kHz RC oscillator. The functions described below only need to be called if an external 32kHz clock source is required. Once an external source has been selected, it is not possible to switch back to the internal RC oscillator.

Also, you could refer to the same chapter, the same document. 

Let me know if you have any further questions.

Regards,

Mario

0 件の賞賛
返信