JN-AN-1245 CoinCell Example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN-AN-1245 CoinCell Example

5,151 Views
matthias_brand
Contributor I

Hi @nxp

In JN-AN-1245 the CoinCell Example for JN5189 is missing. It is mentioned in the documents but the actual source directories are empty.

Could you provide this?

So far I successfully implemented my zigbee application using the DimmerSwitch Example included in JN-AN-1245 and would like to take the next step by switching to the CoinCell Example as my pcb is only driven by a CoinCell.

 

Thank you.

 

BR

Matthias

 

Labels (2)
0 Kudos
Reply
6 Replies

5,034 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @matthias_brand,

I hope you are doing.

I send you a message internally for the requested code.

Regards,

Mario

0 Kudos
Reply

4,713 Views
talhamir49
Contributor III

Hi @mario_castaneda 

I'm working on the JN-AN1246 example and now I want to shift my circuit to coin cell. Can you please send me a coin cell example?

 

Regards,

Talha

0 Kudos
Reply

5,080 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Matthias,

I am sorry for my late reply. I am working on the code that you are requesting.

Regards,

Mario

0 Kudos
Reply

5,097 Views
matthias_brand
Contributor I

@mario_castaneda  any update?

0 Kudos
Reply

5,127 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @matthias_brand,

 

I hope you are doing great. Did you download the AN from the JN5189/88? What are the directories that you are seeing empty?

Then, you could define the #ifdef CoinCellSwitch to enable the coin cell feature.

Let me know if you have any other questions.

Regards,

Mario

0 Kudos
Reply

5,123 Views
matthias_brand
Contributor I

Hi @mario_castaneda 

 

I downloaded it via https://www.nxp.com/webapp/sps/download/license.jsp?colCode=JN-AN-1245.

The archive contains the following directories:

 Directory of C:\Users\matth\Downloads\JN-AN-1245 (1)\JN-AN-1245

17/08/2020  03:58    <DIR>          .
17/08/2020  03:58    <DIR>          ..
17/08/2020  03:56    <DIR>          Binaries
17/08/2020  03:57    <DIR>          ColorSceneController
17/08/2020  03:57    <DIR>          Common
17/08/2020  03:56    <DIR>          Common_Controller
17/08/2020  03:55    <DIR>          Common_Switch
17/08/2020  03:56    <DIR>          DimmerSwitch
17/08/2020  03:56    <DIR>          Doc
17/08/2020  03:55    <DIR>          GpEhSwitch
17/08/2020  03:56    <DIR>          mcux
17/08/2020  03:57    <DIR>          NFC
17/08/2020  03:57    <DIR>          RemoteControlGUI
14/08/2020  05:37                 5 Version.txt
               1 File(s)              5 bytes
              13 Dir(s)  43.626.840.064 bytes free

 

Thereby the directories "CoinCellSwitch" and "Common_CoinCellSwitch "are missing.

 

BR

Matthias

0 Kudos
Reply