JN AN 1216 GreenPower Rx Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN AN 1216 GreenPower Rx Error

ソリューションへジャンプ
3,707件の閲覧回数
seunghokims
Contributor III

Hi

JN AN 1216_ ZigbeeNodeControlBridgeCoordinator_GP_Proxy  cannot receive green power.

It is received before starting the Start Network. (APP_vControlNodeStartNetwork() )

Once the network is created, green power cannot be received.

 

how do i solve it ?

 

If it is set to  sBDB.sAttrib.u8bdbCommissioningMode = 0; 

and network creation fails, green power is received.

 

thanks

0 件の賞賛
返信
1 解決策
3,667件の閲覧回数
seunghokims
Contributor III

Hi mario,

When I double-checked to provide the log, it turned out to be successful.

thanks

Regards,

seungho

元の投稿で解決策を見る

4 返答(返信)
3,691件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @seunghokims,

I hope you are doing great.

Just to confirm, did you define the Green power support in the makefile?

GP_SUPPORT = 1

Regards,

Mario

0 件の賞賛
返信
3,683件の閲覧回数
seunghokims
Contributor III

Hi Mario

 

Yes

I defined GP_SUPPORT = 1 .

so
After setting the Zigbee Node Control Bridge Coordinator channel,
Receive green power data generated from JN-AN 1219 EH_Switch.

--> After running Start Network in Zigbee Node Control Bridge Coordinator
Cannot receive green power data.

 

It is received before starting the Start Network.

how do i solve it

Regards,

0 件の賞賛
返信
3,680件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @seunghokims,

Is it possible that you could provide the sniffer log of this issue?

Also, is it possible that you could provide the terminal log for the devices that you have?

Regards,

Mario

0 件の賞賛
返信
3,668件の閲覧回数
seunghokims
Contributor III

Hi mario,

When I double-checked to provide the log, it turned out to be successful.

thanks

Regards,

seungho