JN-AN-1216 Build Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN-AN-1216 Build Error

2,105件の閲覧回数
1102390310
Contributor I

SDK: JN-SW-4170  Build Number 1840

JN-AN-1216 version 1011

As follows:

pastedImage_1.png

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,012件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Lewin, I hope you're doing well!

 

Could you please check if the binary files are being saved to the project?

If the files are being generated successfully, they should be located in the Build/ZigbeeNodeControlBridge folder of your project.

 

If they're not being generated, could you please try doing a project clean, and then building the project again?

 

Please let me know if you have further issues.

 

Best regards,

Sebastian

0 件の賞賛
返信

2,012件の閲覧回数
1102390310
Contributor I

Hi,

SDK: JN-SW-4170  Build Number 1840

JN-AN-1216 version 1011

I wanted to use the Memsize Tool to see the memory usage of the project.

The following exection statement is in the makefile:

pastedImage_1.png

Compile the project, execute the above statement, and get the following error:

pastedImage_2.png

Lewin

0 件の賞賛
返信

2,012件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Lewin,

 

The parameter error you're seeing is debug information only, and should be ignored. The binary files are being generated successfully in the path mentioned in the previous reply.

 

The output for memsize.exe is being logged in the "text data bss dec hex filename" table printed in the screen capture you took.

 

Please let me know if there's any other information you need.

 

Best regards,

Sebastian

0 件の賞賛
返信