JN-AN-1216 Build Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN-AN-1216 Build Error

2,123 Views
1102390310
Contributor I

SDK: JN-SW-4170  Build Number 1840

JN-AN-1216 version 1011

As follows:

pastedImage_1.png

Labels (1)
0 Kudos
Reply
3 Replies

2,030 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Lewin, I hope you're doing well!

 

Could you please check if the binary files are being saved to the project?

If the files are being generated successfully, they should be located in the Build/ZigbeeNodeControlBridge folder of your project.

 

If they're not being generated, could you please try doing a project clean, and then building the project again?

 

Please let me know if you have further issues.

 

Best regards,

Sebastian

0 Kudos
Reply

2,030 Views
1102390310
Contributor I

Hi,

SDK: JN-SW-4170  Build Number 1840

JN-AN-1216 version 1011

I wanted to use the Memsize Tool to see the memory usage of the project.

The following exection statement is in the makefile:

pastedImage_1.png

Compile the project, execute the above statement, and get the following error:

pastedImage_2.png

Lewin

0 Kudos
Reply

2,030 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Lewin,

 

The parameter error you're seeing is debug information only, and should be ignored. The binary files are being generated successfully in the path mentioned in the previous reply.

 

The output for memsize.exe is being logged in the "text data bss dec hex filename" table printed in the screen capture you took.

 

Please let me know if there's any other information you need.

 

Best regards,

Sebastian

0 Kudos
Reply