***JLink Error: Could not start CPU core. (ErrorCode: -2)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

***JLink Error: Could not start CPU core. (ErrorCode: -2)

5,292件の閲覧回数
wuhanpin
Contributor I

Target info:
------------
Device: QN9080C
VTarget = 3.300V
State of Pins:
TCK: 0, TDI: 0, TDO: 1, TMS: 0, TRES: 1, TRST: 1
Hardware-Breakpoints: 6
Software-Breakpoints: 8192
Watchpoints: 4
JTAG speed: 200 kHz

***JLink Error: Could not start CPU core. (ErrorCode: -2)
***JLink Error: Can not read register 15 (R15) while CPU is running
***JLink Error: Can not read register 20 (CFBP) while CPU is running
***JLink Error: CPU is not halted
***JLink Error: Can not read register 15 (R15) while CPU is running
Full Chip Erase Failed!
Error: Flash Download failed - "Cortex-M4"
Flash Load finished at 12:18:04

使用开发板可以正常烧些。电路部分检查也没有问题. pin33管脚(chip_mode) 如果接GND,SWD 就找不到核心了。

不知道问题

0 件の賞賛
返信
1 返信

2,546件の閲覧回数
Ekta01
Contributor I

same error message.

Any solution on this?

0 件の賞賛
返信