Issue about KW45 dual image boot enable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue about KW45 dual image boot enable

1,458 Views
FVT23029
Contributor I

I refer to "15.2.3.1 Dual image boot" in KW45RM.pdf and using Secure Provisioning Tool v8.0 to set ROMCFG/IFR0 as following:

螢幕擷取畫面 2024-08-20 135325.png螢幕擷取畫面 2024-08-20 135258.png螢幕擷取畫面 2024-08-20 135306.png

and I prepared two binaries from the "kw45b41zevk_hello_world", one will show "Hello World 1" and another one is "Hello World 2"

I flashed the "Hello World 1" into address 0x0 and then flashed "Hello World 2" into address 0x80000 but I always got "Hello World 1" message after boot up.

Does any steps miss with my method?

0 Kudos
Reply
1 Reply

1,396 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. I would recommend checking this Application Note: "AN14109: KW45 and K32W148 Secure Boot Using the SEC Tool".

 

This file is under Secure Files. If you have an active NDA, you could request it directly on NXP.com.

Secure Access Rights | NXP Semiconductors

 

Could you please follow the process?

 

Also, I would recommend checking the Secure Access Rights FAQs | NXP Semiconductors

 

Regards,

Ricardo

0 Kudos
Reply