Issue about KW45 dual image boot enable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue about KW45 dual image boot enable

1,457件の閲覧回数
FVT23029
Contributor I

I refer to "15.2.3.1 Dual image boot" in KW45RM.pdf and using Secure Provisioning Tool v8.0 to set ROMCFG/IFR0 as following:

螢幕擷取畫面 2024-08-20 135325.png螢幕擷取畫面 2024-08-20 135258.png螢幕擷取畫面 2024-08-20 135306.png

and I prepared two binaries from the "kw45b41zevk_hello_world", one will show "Hello World 1" and another one is "Hello World 2"

I flashed the "Hello World 1" into address 0x0 and then flashed "Hello World 2" into address 0x80000 but I always got "Hello World 1" message after boot up.

Does any steps miss with my method?

0 件の賞賛
返信
1 返信

1,395件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. I would recommend checking this Application Note: "AN14109: KW45 and K32W148 Secure Boot Using the SEC Tool".

 

This file is under Secure Files. If you have an active NDA, you could request it directly on NXP.com.

Secure Access Rights | NXP Semiconductors

 

Could you please follow the process?

 

Also, I would recommend checking the Secure Access Rights FAQs | NXP Semiconductors

 

Regards,

Ricardo

0 件の賞賛
返信