Is there a way to restart Co-ordinator in such a way that remote nodes do not need to re-enter the network?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a way to restart Co-ordinator in such a way that remote nodes do not need to re-enter the network?

1,182 Views
xleaderx
Contributor I

Hello guys!
I have a question.
I'm using the ZigBee JN5168 module in our project.
My software uses the JN-SW-4170 SDK.
The software is based on the example JN-AN-1229-ZBPro-Application-Template using the ZBPro stack.

I often have situations when it is necessary to restart the Co-ordinator without restarting the entire ZigBee network.
But, in this case, it is no longer possible to communicate with the remote nodes.
Communication is restored only when the nodes re-enter the network.

Is there a way to restart Co-ordinator in such a way that remote nodes do not need to re-enter the network?

Labels (3)
0 Kudos
Reply
1 Reply

1,137 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

By default, the JN-AN-1229 is not saving the Zigbee network information. That is the reason for the devices need to join a new network. You could take a look to the JN-AN-1217 and look t the save process.

Regards,

Mario

0 Kudos
Reply