Is it require to add cluster in router device?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is it require to add cluster in router device?

跳至解决方案
2,692 次查看
bhautik_ruparel
Contributor II

Hello Support Team,

I have used one Coordinator, Router and End device and configured cluster on Coordinator and End device side as per application.

I configure Dimmable Light [0x0101] as a router.

So Is it require to add/configure cluster [i.e. Group, Scenes, Level Control, On/Off cluster, etc.] on router side? 

Regards,

Bhautik

标记 (1)
0 项奖励
回复
1 解答
2,625 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @bhautik_ruparel,

In this case, the router will be sent the packet to the coordinator, if the destination address is the coordinator, but you are right the router doesn't need any cluster for this.

Regards,

Mario

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,626 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @bhautik_ruparel,

In this case, the router will be sent the packet to the coordinator, if the destination address is the coordinator, but you are right the router doesn't need any cluster for this.

Regards,

Mario

0 项奖励
回复
2,650 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @bhautik_ruparel,

In this case, if you do not add this cluster functionality, the router can not respond and support some commands that the coordinator could request. It will depend on your application

Regards,

Mario

0 项奖励
回复
2,640 次查看
bhautik_ruparel
Contributor II

Hello @mario_castaneda 

Thanks for your response.

As per our application I have configure router [Dimmable Light] as a range extender and also just routing the packet from end device to coordinator and vice versa. 

So In this condition no need to require to add or configure cluster. Is that my understanding right?

Regards,

Bhautik 

0 项奖励
回复