Information microcontroller with Time of Flight.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Information microcontroller with Time of Flight.

1,932 Views
nikivendola
Contributor III

Good morning,
i would build a wireless application that allows me to detect the position of a transmitter by calculating the phase of the signal arriving on two antennas placed in rx at some distance.

If not mistaken for managing an application of this type I need to detect Time of Flight.
For which they are looking for a microcontroller which allows to detect Time of Flight.

The working frequency is 2.4GHz.

I found the micro JN5148-001 of your competitor: http://www.nxp.com/documents/data_sheet/JN5148.pdf.

This allows the Time of Flight.

Can you help me find a micro appropriate for your production?
Can you give me any suggestions to make this application?

Thank you and greetings

Labels (1)
0 Kudos
Reply
1 Reply

1,406 Views
mihaidragnea
NXP Employee
NXP Employee

Hi Niki,

At this point Freescale doesn't have any wireless MCU that implements Time of Flight.

On the other hand, NXP and Freescale should soon merge and become one single company (NXP) so I encourage you to use JN5148.

I am confident that you will find the right support on NXP website/forums/etc.

Regards,

Mihai

0 Kudos
Reply