Implementing serial protocol between host and control bridge.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implementing serial protocol between host and control bridge.

1,870 Views
kousikbarathwaj
Contributor I

In JN-AN-1194 (Zigbee Iot gateway application note) the document for control bridge, NXP have specified serial protocol and command sets to interact with the control bridge (zigbee module connected to the host) from the host through serial connection. In the accompanying documents for host they have used Jennet ip for translation between IPV6 and WPAN packets.

In our project there is no need for IPV6 translations.   From the linux host we have to interact with the control bridge(zigbee module connected to the host) through serial protocol.  Please suggest me on how this can be implemented.

Thanks in advance.

Labels (2)
0 Kudos
Reply
0 Replies