Implement RF Communication between Two JN5168 Module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Implement RF Communication between Two JN5168 Module

4,308件の閲覧回数
dheerajsawant
Contributor V

Hello Friends, 

i just familiar with JN5168-001-M00 module. 

i have learn how to compile and build a code and create binary files.

credit goes to NXP community. 

Now i have come to my main project which is RF Based. 

1) i have  to communicate 2 JN5168 Module with each other.

2) Basic task is to send "STRING" from one module to another and vice versa.

I dont to how to start. Even i dont have any sample example for it. 

please needed your help. if you have sample code regarding this concept. 

Then please provide.

Thank You for your time.

5 返答(返信)

3,877件の閲覧回数
adamjacob
Contributor II

Calling the makers and experts interested in using Zigbee via NXP JN5168 modules, please join the facebook group so we can help each other:)
https://goo.gl/DeYbC6
Cheers

3,877件の閲覧回数
davidashraf
Contributor V

Hello Dheeraj Sawant

Have a look at this discussion . I believe It includes what you are asking for
Simple Data transfer 

Also for full API please refer to stack user guide according to the stack you are using from 
Support Resources for JN516x MCUs|NXP 

Regards

0 件の賞賛
返信

3,877件の閲覧回数
dheerajsawant
Contributor V

Hello Sir, 

Thank You very much for your reply.

Where can i download Application Note related to Simple data transfer using RF Communication for JN5168 Module.

Thank you for your time.

0 件の賞賛
返信

3,877件の閲覧回数
davidashraf
Contributor V

Hello , 

It's more of a general code that can be used within any code 

I was working with JN-AN-1229 based on ZigBee 3.0 stack

It would also work with JN - AN - 1184 based on ZigBee pro stack 

You can find all resources from here 

Support Resources for JN516x MCUs|NXP 

Please let me know if there're any further questions 

Regards

0 件の賞賛
返信

3,877件の閲覧回数
dheerajsawant
Contributor V

Hello mario_castaneda , dereksnell

Thank you for your help 

you solved my previous problems. 

right now i am going to start A project from basic. I don't how to start this  project. so required your help.

please read my above message 

if there are API, Sample code or any suggestion related to RF communication project please let me know.

Thank You for your time.

0 件の賞賛
返信