IW612/IW611 MAYA-W2 Module Bluetooth bring up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IW612/IW611 MAYA-W2 Module Bluetooth bring up

3,335 Views
nifroidl
Contributor II

I am using the MAYA-W2 module from u-blox for a WiFi Bluetooth Adapter. Since there is the IW611/IW612 populated, maybe some of you can help me. I can easily bring up WiFi using the mwifiex driver and imx-firmware for IW612 but I am not able to bring up Bluetooth:

root@phyboard-pollux-imx8mp-3:~# hciattach /dev/ttymxc2 any 115200 flow
Setting TTY to N_HCI line discipline
Device setup complete
root@phyboard-pollux-imx8mp-3:~# [ 68.060988] Bluetooth: hci0: command 0x1003 tx timeout
[ 70.076990] Bluetooth: hci0: command 0x1001 tx timeout
[ 72.092997] Bluetooth: hci0: command 0x1009 tx timeout
root@phyboard-pollux-imx8mp-3:~# hciconfig hci0 up
[ 88.316175] Bluetooth: hci0: command 0x1003 tx timeout
[ 90.332097] Bluetooth: hci0: command 0x1001 tx timeout
[ 92.348038] Bluetooth: hci0: command 0x1009 tx timeout
Can't init device hci0: Connection timed out (110)
root@phyboard-pollux-imx8mp-3:~# hcitool dev
Devices:
root@phyboard-pollux-imx8mp-3:~#

Can someone help me? Do you havdthis issue already?

Labels (1)
Tags (2)
0 Kudos
Reply
5 Replies

2,548 Views
pratham_malaviya
Contributor III

HI @nifroidl ,
Were you able to solve this issue?
I am stuck at the same.

0 Kudos
Reply

2,519 Views
nifroidl
Contributor II

@pratham_malaviya Yes. In my case it was an HW issue. I had to switch RTS and CTS signal for UART. After that I was able to get the BT interface running

0 Kudos
Reply

2,503 Views
pratham_malaviya
Contributor III

@nifroidl In my case when i don't use flow control (RTS unconnected / Module CTS grounded) the interface work. Which hardware connection did you used to make it work?

0 Kudos
Reply

2,341 Views
nifroidl
Contributor II

@pratham_malaviya Maybe this is your issue. Do you have teh Flow Control Pins available? I think I tried to use the chip without Flow Control and it didn't work.

0 Kudos
Reply

3,316 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

I will contact you in the other case.

Regards,
Daniel.

0 Kudos
Reply