IAS Zone Cluster

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IAS Zone Cluster

3,121件の閲覧回数
rostislav
Contributor III

Hello everybody,

I use Freescale BeeKit + IAR compiler to create a security device. It should support alarm (9) and IAS Zone (500) clusters. Enabling these clusters I got linker errors:

Error[Li005]: no definition for "gIASZoneTable" [referenced from D:\projects\zigbee_module\coordinator_module\coordinator_module\Ha GenericApp\Release\Obj\ZclSecAndSafe.o]

Error[Li005]: no definition for "gIndexInIASZoneTable" [referenced from D:\projects\zigbee_module\coordinator_module\coordinator_module\Ha GenericApp\Release\Obj\ZclSecAndSafe.o]

Could anybody help me finding where gIASZoneTable and gIndexInIASZoneTable are defined?

Thank you in advance.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,683件の閲覧回数
rostislav
Contributor III

Thanks Ovidiu,

That makes sence

0 件の賞賛
返信

2,683件の閲覧回数
rostislav
Contributor III

Hi Ovidiu,

I have 3.1.1 version setup on my PC. It doesn't have the application as well. By the way these old versions are for obsolete chips. For Kinetis chip you need download the latest version from the NXP website. Unfortunately your responses are useless.

NXP support: could anybody help me please?

0 件の賞賛
返信