IAS Zone Cluster

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IAS Zone Cluster

3,066 Views
rostislav
Contributor III

Hello everybody,

I use Freescale BeeKit + IAR compiler to create a security device. It should support alarm (9) and IAS Zone (500) clusters. Enabling these clusters I got linker errors:

Error[Li005]: no definition for "gIASZoneTable" [referenced from D:\projects\zigbee_module\coordinator_module\coordinator_module\Ha GenericApp\Release\Obj\ZclSecAndSafe.o]

Error[Li005]: no definition for "gIndexInIASZoneTable" [referenced from D:\projects\zigbee_module\coordinator_module\coordinator_module\Ha GenericApp\Release\Obj\ZclSecAndSafe.o]

Could anybody help me finding where gIASZoneTable and gIndexInIASZoneTable are defined?

Thank you in advance.

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

2,628 Views
rostislav
Contributor III

Thanks Ovidiu,

That makes sence

0 Kudos
Reply

2,628 Views
rostislav
Contributor III

Hi Ovidiu,

I have 3.1.1 version setup on my PC. It doesn't have the application as well. By the way these old versions are for obsolete chips. For Kinetis chip you need download the latest version from the NXP website. Unfortunately your responses are useless.

NXP support: could anybody help me please?

0 Kudos
Reply