How to use push button of FRDM-KW36 to connect with peripheral device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use push button of FRDM-KW36 to connect with peripheral device

2,025 次查看
sihanchen
Contributor III

Hello ~ 

          I am working on FRDM-KW36 development board and use (frdmkw36_wireless_examples_bluetooth_w_uart_freerots) SDK to build code by MCUXpresso IDE. 

I have prepared a BLE peripheral device and I would like to use the push button of FRDM-KW36 to connect with the peripheral device, but I don't know how to use push button to select the specific peripheral device, Do I need to modify NXP's SDK for to use auto connection of BLE. Can anyone tell me if you know. 

Thanks. 

标签 (2)
3 回复数

1,911 次查看
sihanchen
Contributor III

Update the question ... 

The FRDM-KW36 default is central role and will scanning and connect with peripheral device automatically when you push scanning button, You will need to use print message to know the status of connection, so I thinks this question can be close. Thanks. 

0 项奖励
回复

1,911 次查看
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Sihan,

Please let me know if you need any more information.

Best regards,

Sebastian

1,911 次查看
sihanchen
Contributor III

Hi All, 

      The Bluetooth Low Energy Demo Application User Guide.pdf only shows how to use the FRDM-KW36 as peripheral device to connect with the NXP's Iot-Toolbox APP (Wireless-UART). I would like to know how to use the FRDM-KW36 as central device and connect with a peripheral device, Does the NXP's Iot-toolsbox APP can configure as a peripheral device and then do the Wireless-UART test ?


Thanks.

0 项奖励
回复