How to use OTA to update the coordinator program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use OTA to update the coordinator program

Jump to solution
3,052 Views
lvdp
Contributor III

Hi:

       We currently use JN5189 to develop a gateway, and JN5189 uses UART1 to communicate with the WIFI chip. We want to upgrade the program of the coordinator via WIFI. What should we do? Is there any routine for reference?

0 Kudos
Reply
1 Solution
3,042 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

I hope you are doing great.

Just to confirm, do you want to update the MCU throught UART interface, am I wrong?

However, you could look at the app_ota_client.c file 

#if (defined OTA_INTERNAL_STORAGE)

You could look at the comments about the flash and the sectors that are used. Unfortunately, we do not provide a bootloader that helps you to implement the update using serial communication.

Look at the JN-AN-1244 to take as reference the OTA update.

Regards,

Mario

View solution in original post

0 Kudos
Reply
2 Replies
3,043 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

I hope you are doing great.

Just to confirm, do you want to update the MCU throught UART interface, am I wrong?

However, you could look at the app_ota_client.c file 

#if (defined OTA_INTERNAL_STORAGE)

You could look at the comments about the flash and the sectors that are used. Unfortunately, we do not provide a bootloader that helps you to implement the update using serial communication.

Look at the JN-AN-1244 to take as reference the OTA update.

Regards,

Mario

0 Kudos
Reply
3,038 Views
lvdp
Contributor III

Hi,mario:

      Yes, we hope to receive the upgrade package sent from the WiFi chip through USART1 and update the coordinator program.Ok, I see, thanks for your reply.

0 Kudos
Reply