How to use OTA to update the coordinator program

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use OTA to update the coordinator program

ソリューションへジャンプ
2,793件の閲覧回数
lvdp
Contributor III

Hi:

       We currently use JN5189 to develop a gateway, and JN5189 uses UART1 to communicate with the WIFI chip. We want to upgrade the program of the coordinator via WIFI. What should we do? Is there any routine for reference?

ラベル(4)
0 件の賞賛
返信
1 解決策
2,783件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

I hope you are doing great.

Just to confirm, do you want to update the MCU throught UART interface, am I wrong?

However, you could look at the app_ota_client.c file 

#if (defined OTA_INTERNAL_STORAGE)

You could look at the comments about the flash and the sectors that are used. Unfortunately, we do not provide a bootloader that helps you to implement the update using serial communication.

Look at the JN-AN-1244 to take as reference the OTA update.

Regards,

Mario

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,784件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

I hope you are doing great.

Just to confirm, do you want to update the MCU throught UART interface, am I wrong?

However, you could look at the app_ota_client.c file 

#if (defined OTA_INTERNAL_STORAGE)

You could look at the comments about the flash and the sectors that are used. Unfortunately, we do not provide a bootloader that helps you to implement the update using serial communication.

Look at the JN-AN-1244 to take as reference the OTA update.

Regards,

Mario

0 件の賞賛
返信
2,779件の閲覧回数
lvdp
Contributor III

Hi,mario:

      Yes, we hope to receive the upgrade package sent from the WiFi chip through USART1 and update the coordinator program.Ok, I see, thanks for your reply.

0 件の賞賛
返信