How to register multiple endpoints

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to register multiple endpoints

2,461件の閲覧回数
836733207
Contributor II

Hello Everyone:

      I am new to Zigbee and I have trouble in register multiple endpoints.
      I can regiser a endpoints and it can word well,however,when I attented to add another,the application go wrong and printf "Alignment error" as the figure showed below.I have already added the definition in .zpscfg,and increased ZCL_NUMBER_OF_ENDPOINTS. I can not figure out what is wrong.
      The code that I used to register endpoints are showed below too,is there any mistake?
      Please, could anyone help me and give some infos?

pastedImage_2.png

pastedImage_1.png

0 件の賞賛
返信
3 返答(返信)

2,347件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,  

I was checking your implementation. Is the sIASCIE a structure type tsHA_IASCIE?

As the ZigBee Home Automation User Guide mentions, this parameter should be a pointer to the structure that will act as storage for all variables related to the device being registered on this endpoint.

What is the status value that you are getting?

Regards,

Mario

0 件の賞賛
返信

2,347件の閲覧回数
836733207
Contributor II

Thanks for your reply!

      Yes,sIASCIE is a structure type tsHA_IASCIE,as I define  “ tsHA_IASCIE   sIASCIE[10]  ”. I think &sIASCIE[0] is an appropriate parameter,is that true?

      The eZCL_Status,the return of the register funtion is E_ZCL_SUCCESS.

      The same error occur when I change to use another function eZHA_RegiserBaseDeviceEndPoint().

      Yesterday,I tried to chose "Erase EEPROM" when programming device,and I succeed in register another endpoint.Howerver,when I tried to add more,the same error occur.

     

Best Regards,

Du

0 件の賞賛
返信

2,347件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Du,

Is there a reason why you are working on IAS Zone?

Did you look at the https://community.nxp.com/docs/DOC-333994

Regards,

Mario

0 件の賞賛
返信