How to increase MAX ATT_MTU size ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to increase MAX ATT_MTU size ?

3,806 Views
rajarathinamlaw
Contributor I

I am using FRDM KW40z dev.board and KW40Z_Connectivity_Software_1.0.1 software for our application development. Here I need increase ATT_MTU size as 512 byte instead of 23(gAttMaxMtu_c = 23) for application but  I changed gAttMaxMtu_c as 512 in ble_constants.h file and after connection application called GattClient_ExchangeMtu(peerDeviceId) function but still MTU exchanged with client RX MTU size is 23. 

Could you please explain how to increase the ATT_MTU maximum size to upload large data? 

0 Kudos
Reply
1 Reply

3,442 Views
neoxiong
NXP Employee
NXP Employee

Hi, Raja

You are not able to change macro in ble_constants.h file as they're hard linked by nxp ble stack. I think whatever the value you modify, the stack still uses 23. 

KW40 is a BLE 4.1 SoC which only support short packet, even you set ATT_MTU to 512, on l2cap level, stack will split it into multiple link layer packets, throughput will get not significant improve (only few bytes overhead get reduced).

And, KW40 is an old device, could you consider switching to KW41? KW41 is BLE 4.2 SoC support Data Length Extension Feature, and very similar to KW40. 

0 Kudos
Reply