How to get rid of on/off transition time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get rid of on/off transition time

1,324 Views
jacco_bezemer
Contributor III

Hello,

I successfully used the JN-AN-1171 demo to make an incandescent light bulb dimmer for a Philips HUE system.

The HUE system is primarily used for Led lighting and when turning the light on or off it uses a transition time to create a soft on/off effect.

Since i use an incandescent bulb i want to get rid of this effect.

Is there a way to get this done at the receiver end?

Kind regards,

Jacco

Labels (2)
0 Kudos
Reply
1 Reply

1,234 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Jacco, I hope you're doing well!

 

The related functions are included in the app_light_interpolation source and header files inside the Common_Light/Source folder. Could you please take a look at these files to see if you can remove them to skip the fading in/out effect?

 

Please let me know if you need any more information.

 

Best regards,

Sebastian

0 Kudos
Reply