How does JN5189 use GINT1 interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How does JN5189 use GINT1 interrupt

781 Views
Tome-mbedded
Contributor II

hello everyone,

I run the sdk driver example JN5189dk6_gint, which uses GINT0

Tomembedded_0-1711988527710.png

I want to use GInT0 and GINT1 because there are two I/O ports that may cause an interrupt at the same time.  but it compiled incorrectly because GINT1 was not defined. Only GINT0 is defined in the example

Tomembedded_1-1711988690702.png

How do I define the GINT1 macro?

thankyou 

 

0 Kudos
Reply
1 Reply

762 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. There is no GINT1. Please refer to section 2.1.2 of the JN5189(T)/JN5188(T) User manual.

 

Regards,

Ricardo

0 Kudos
Reply