How does JN5169 reset the network layer or MAC layer?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How does JN5169 reset the network layer or MAC layer?

1,482 次查看
1948396491
Contributor II

Hello, may I ask whether the JN5169 reset CPU resets the network layer and MAC layer?In addition, is there any way to reset the network layer and the MAC layer respectively?Or directly reset the network layer and MAC layer?

0 项奖励
回复
2 回复数

1,469 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @1948396491,

Please look at the 3.1 MAC Reset for more details also look at the example 3.1.2 Reset Example

https://www.nxp.com/docs/en/user-guide/JN-UG-3024.pdf 

Regards,

Mario

0 项奖励
回复

1,370 次查看
1948396491
Contributor II

Hello, the chip I use is JN5169, and the routine uses JN-AN-1217-ZigBee-3-0-Base-Device.The SDK version is 1840.

The problem I encountered was that after the reset of my software, I could not recover after receiving instruction error. After a while, the watchdog reset, and then receiving instruction error again.

I would like to ask three questions:

First: Why do you have the problem of instruction error?

Second: how to find and solve the problem?

Third, how to analyze the address information of STACK DUMP printed by the software after an exception occurs and what are the meanings of those variables in front of it?

1948396491_0-1615511791196.png

 

0 项奖励
回复