How do uart communication?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do uart communication?

ソリューションへジャンプ
5,526件の閲覧回数
rla00220
Contributor III

I am using wct1013a.

I know wct1013a supports uart and i2c communication.

However, there is no uart communication example in the demo version.

Can I get an example of uart communication?

1 解決策
5,206件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Semikim,

 

Glad to know that you find and solve the problem.

元の投稿で解決策を見る

6 返答(返信)
5,206件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately, I don’t think that we have any available UART communication example in demo version for the WCT1013A, I can check with the applications Engineers, but in order to do that I need to know more details about the customer and the application, can you please answer the following questions, please? This would give us a better understanding of your project: 
1. Name of the customer Company:

  1. Website of the company:
  2. Market Segment:
    4. Name of the project:
    5. End Product/ Product: 
    6. Project Stage: 
    7. Annual Production Volume: 
    8. Project Details: 
    9. Prod Start Dt: 

 

I’ll wait for your answer in order to contact the applications engineers to answer to your question.

Regards,

Jose

0 件の賞賛
返信
5,206件の閲覧回数
rla00220
Contributor III

hello???

I was successful.

The problem was in defined

It was possible to change the define to consol mode..

Thanks for your help.

2019년 4월 2일 (화) 오후 3:42, 김세미 <[email protected]>님이 작성:

hi.

i found Uart = SCi c, h code.

but... it not working.

I want to send wct's Rx status as uart ch0.

what can i do??

help me plz... thanks.

>

2019년 3월 30일 (토) 오전 6:51, reyes <[email protected]>님이 작성:

>> NXP Community

>> <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

>> Re: How do uart communication?

>>

>> reply from Jose Alberto Reyes Morales

>> <https://community.nxp.com/people/reyes?et=watches.email.thread> in *Wireless

>> Connectivity* - View the full discussion

>> <https://community.nxp.com/message/1132603?commentID=1132603&et=watches.email.thread#comment-1132603>

>>

0 件の賞賛
返信
5,207件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Semikim,

 

Glad to know that you find and solve the problem.

5,206件の閲覧回数
rla00220
Contributor III

hi.

i found Uart = SCi c, h code.

but... it not working.

I want to send wct's Rx status as uart ch0.

what can i do??

help me plz... thanks.

2019년 3월 30일 (토) 오전 6:51, reyes <[email protected]>님이 작성:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: How do uart communication?

reply from Jose Alberto Reyes Morales

<https://community.nxp.com/people/reyes?et=watches.email.thread> in *Wireless

Connectivity* - View the full discussion

<https://community.nxp.com/message/1132603?commentID=1132603&et=watches.email.thread#comment-1132603>

0 件の賞賛
返信
5,206件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Semikim,

 

Is this Uart = ACi c, h code a NXP authorized code for the WCT1013A? If so, can you please point me to the site you found it, please?

 

Otherwise I’m afraid that if the code was not made from NXP, we would not be able to support it.


Regards,
Jose

0 件の賞賛
返信
5,206件の閲覧回数
rla00220
Contributor III

Yes.

it was sample code form nxp.

You can download it here. thanks.

https://www.nxp.com/products/power-management/wireless-power/15-watt-wireless-charging-transmitter-i...

2019년 4월 3일 (수) 오전 2:01, reyes <[email protected]>님이 작성:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: How do uart communication?

reply from Jose Alberto Reyes Morales

<https://community.nxp.com/people/reyes?et=watches.email.thread> in *Wireless

Connectivity* - View the full discussion

<https://community.nxp.com/message/1133856?commentID=1133856&et=watches.email.thread#comment-1133856>

0 件の賞賛
返信