Hi,
I am playing around to see whether it is possible to transfer information between 2 CLEV6630B (i.e. NFC P2P communication). I have 2 CLEV6630B but I only have 1 LPC-LINK 2. I didn't find a way to run the program on CLEV6630B without LPC-LINK 2.
I can understand that when deploying the code to CLEV6630B, there is a need to run a middleware to transfer/decode my script into the target device. However, I cannot understand why there is any necessity to keep the link board all the time while the device is running. Is there any way that I can run my program on CLEV6630B without consistently connecting to an LPC-LINK 2 board?
Thanks a lot in advance!
Haifeng.
解決済! 解決策の投稿を見る。
Hello @Haifeng ,
I assume you are using MCUXpresso IDE , then you may find the projects from NFC reader library contain Debug and Release version, the Release version can run standalone without connected to LPC-LINK 2 after the CLEV6630B programmed.
Hope that makes sense,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello @Haifeng ,
I assume you are using MCUXpresso IDE , then you may find the projects from NFC reader library contain Debug and Release version, the Release version can run standalone without connected to LPC-LINK 2 after the CLEV6630B programmed.
Hope that makes sense,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks for your reply!
That exactly solved my problem. Thanks a lot.
FYI, if there is anyone who finds this thread and builds the release version with the error said cannot find lpc_board_nxp_lpcxpresso_1769, you can try to build that project in the library before building your own project.
Best Regards,
Haifeng.
Hi Haifeng,
It's great to know this issue got solved on your side! and Thanks for the sharing!
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------