How can I implement Connection Parameters Request Procedure on QN908x as Peripheral device?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I implement Connection Parameters Request Procedure on QN908x as Peripheral device?

ソリューションへジャンプ
4,424件の閲覧回数
daisuke
Contributor II

Hello,

I would like to code "Connection Parameters Request Procedure" to QN908x as a peripheral role.  Has anyone already implemented this?

I was searching sample codes for this, but I could not find any (even though there are many other sample code for services/profiles).

If I could get any sample code/snippet for this, it would be much appreciated.

Thanks,

Daisuke  

1 解決策
4,089件の閲覧回数
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Daisuke,

You can use the Gap_UpdateConnectionParameters() API from the peripheral to issue a Connection Parameter Update Request, but it will depend on the master if it will accept or reject the request.

Example:

Gap_UpdateConnectionParameters(mPeerDeviceId, gGapDefaultMinConnectionInterval_d , gGapDefaultMaxConnectionInterval_d, gGapDefaultConnectionLatency_d, gGapDefaultSupervisionTimeout_d, gGapConnEventLengthMin_d, gGapConnEventLengthMax_d);

Regards,

元の投稿で解決策を見る

3 返答(返信)
4,090件の閲覧回数
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Daisuke,

You can use the Gap_UpdateConnectionParameters() API from the peripheral to issue a Connection Parameter Update Request, but it will depend on the master if it will accept or reject the request.

Example:

Gap_UpdateConnectionParameters(mPeerDeviceId, gGapDefaultMinConnectionInterval_d , gGapDefaultMaxConnectionInterval_d, gGapDefaultConnectionLatency_d, gGapDefaultSupervisionTimeout_d, gGapConnEventLengthMin_d, gGapConnEventLengthMax_d);

Regards,

4,089件の閲覧回数
joachimk
Contributor II

Where to call this function? Do you have example code?

0 件の賞賛
返信
4,089件の閲覧回数
daisuke
Contributor II

Hello Gerardo,

Thank you very much for your reply.

Now, My 9080 as peripheral can send connection parameter update request to the peer.

Best Regards,

Daisuke