How can I implement Connection Parameters Request Procedure on QN908x as Peripheral device?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How can I implement Connection Parameters Request Procedure on QN908x as Peripheral device?

跳至解决方案
4,473 次查看
daisuke
Contributor II

Hello,

I would like to code "Connection Parameters Request Procedure" to QN908x as a peripheral role.  Has anyone already implemented this?

I was searching sample codes for this, but I could not find any (even though there are many other sample code for services/profiles).

If I could get any sample code/snippet for this, it would be much appreciated.

Thanks,

Daisuke  

1 解答
4,138 次查看
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Daisuke,

You can use the Gap_UpdateConnectionParameters() API from the peripheral to issue a Connection Parameter Update Request, but it will depend on the master if it will accept or reject the request.

Example:

Gap_UpdateConnectionParameters(mPeerDeviceId, gGapDefaultMinConnectionInterval_d , gGapDefaultMaxConnectionInterval_d, gGapDefaultConnectionLatency_d, gGapDefaultSupervisionTimeout_d, gGapConnEventLengthMin_d, gGapConnEventLengthMax_d);‍‍

Regards,

在原帖中查看解决方案

3 回复数
4,139 次查看
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Daisuke,

You can use the Gap_UpdateConnectionParameters() API from the peripheral to issue a Connection Parameter Update Request, but it will depend on the master if it will accept or reject the request.

Example:

Gap_UpdateConnectionParameters(mPeerDeviceId, gGapDefaultMinConnectionInterval_d , gGapDefaultMaxConnectionInterval_d, gGapDefaultConnectionLatency_d, gGapDefaultSupervisionTimeout_d, gGapConnEventLengthMin_d, gGapConnEventLengthMax_d);‍‍

Regards,

4,138 次查看
joachimk
Contributor II

Where to call this function? Do you have example code?

0 项奖励
回复
4,138 次查看
daisuke
Contributor II

Hello Gerardo,

Thank you very much for your reply.

Now, My 9080 as peripheral can send connection parameter update request to the peer.

Best Regards,

Daisuke