Hi @mario_castaneda,
Thanks for the quick reply.
Please find below answers:
1) 0x80 error code is visible on Control Bridge or ZED that joined the network?
Ans: 0x80 error code is visible on the Control Bridge Side.
2) when does 0x80 error code visible: during ZED commissioning or after ZED joined the network?
Ans: Mostly 0x80 error code is visible when I power cycle the ZED and ZED Sends "Device Announce" Message to the Control Bridge. (after 4 to 5 retries of power cycle the ZED, Control Bridge stuck with the error code 0x80)
3) power cycle only on Control Bridge without ZEDs been powered cycled?
Ans: Here, I am power cycle the ZED not the Control Bridge.
Please refer attached .zpscfg file which we are using and also, refer to the attached logs when the error occurs.