Gateway get some error in middle scale network

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Gateway get some error in middle scale network

1,991 次查看
leoxie
Contributor I

Dear All,

  our gateway was get follow Error in sometime, How can I to solve it?   Thanks verymuch.

 图片1.png

QQ截图20180918140153.png

By the way: I was joined Twenty Router and Fifty-Three Sleep device in the network.

标签 (2)
0 项奖励
回复
3 回复数

1,877 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Leo Xie,

Could you please confirm the part number that you are working on? Could you please provide more information about your project?

Regards,

Mario

0 项奖励
回复

1,877 次查看
leoxie
Contributor I

Hi Mario,

    Thanks very much for your reply.

    The gateway working on JN5169 and our host, I saw the error that made me feel the RAM maybe is not enough.

     The RAM and FLASH size are showed as below: 

pastedImage_1.png

    The  remaining RAM is : (28725 + 2500) / 1024 ≈ 30.5K    Am I right?

    And what more information woud you want, Please feel free tell me.

   Thanks Again.

0 项奖励
回复

1,877 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Leo Xie,

The Zigbee coordinator control bridge that you are working on has a lot of cluster support. So, if you are not working with some cluster and domains, you can delete the ones that are consuming a lot of RAM.

When you are seeing this error, is the applications stopping all the process.

Regards,

Mario

0 项奖励
回复