FRDM-KW41Z Development board - Onboard RX/TX voltage level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KW41Z Development board - Onboard RX/TX voltage level

Jump to solution
2,785 Views
dvdsosa
Contributor II

Hello,

I have just bought an FRDM-KW41Z dev kit. 

The dev board has an Arduino R3 compatible connector (for shields or individual cables). 

I can not find if the serial RX/TX pins of this socket (HDR pin 1 (PTC6) and pin 2 (PTC7)) are TTL compatible or 3V3.

I see in the schematics that they are connected directly to the uP (MKW41Z512VHT4 MCU). 

Please, can anyone tell me which are the RX/TX voltage levels in such board?

Kind regards,

David.

0 Kudos
Reply
1 Solution
2,766 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi david_sosa,

  KW41 is 3.3V.

  As I know, some TTL-USB tool can select 3.3V, this is an example:

 

image.png

 

Wish it helps you!

Best Regards,

Kerry

View solution in original post

0 Kudos
Reply
3 Replies
2,772 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi david_sosa,

  PTC6, PTC7 which is the UART0-TX and UART_RX pin, it is the 3.3V TTL pin.

   So, you also can find a TTL-USB tool to connect that pin, please note, the TTL-USB tool also need to provide the 3.3V to the UART TLL pins.

 

Wish it helps you!

If you still have questions about it, please kindly let me know!

Best Regards,

Kerry

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-----------------------------------------------------------------------------

0 Kudos
Reply
2,769 Views
dvdsosa
Contributor II

Hello Kerry,

I'm sorry, but with your answer, I still have the doubt.

Given that TTL is 5V (it is not the same as 3.3V), then, at which voltage works the UART from the FRDM-KW41Z? 5V or 3.3V?

Regards,

David.

0 Kudos
Reply
2,767 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi david_sosa,

  KW41 is 3.3V.

  As I know, some TTL-USB tool can select 3.3V, this is an example:

 

image.png

 

Wish it helps you!

Best Regards,

Kerry

0 Kudos
Reply