FRDM-KW41Z Development board - Onboard RX/TX voltage level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KW41Z Development board - Onboard RX/TX voltage level

ソリューションへジャンプ
2,771件の閲覧回数
dvdsosa
Contributor II

Hello,

I have just bought an FRDM-KW41Z dev kit. 

The dev board has an Arduino R3 compatible connector (for shields or individual cables). 

I can not find if the serial RX/TX pins of this socket (HDR pin 1 (PTC6) and pin 2 (PTC7)) are TTL compatible or 3V3.

I see in the schematics that they are connected directly to the uP (MKW41Z512VHT4 MCU). 

Please, can anyone tell me which are the RX/TX voltage levels in such board?

Kind regards,

David.

0 件の賞賛
返信
1 解決策
2,752件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi david_sosa,

  KW41 is 3.3V.

  As I know, some TTL-USB tool can select 3.3V, this is an example:

 

image.png

 

Wish it helps you!

Best Regards,

Kerry

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,758件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi david_sosa,

  PTC6, PTC7 which is the UART0-TX and UART_RX pin, it is the 3.3V TTL pin.

   So, you also can find a TTL-USB tool to connect that pin, please note, the TTL-USB tool also need to provide the 3.3V to the UART TLL pins.

 

Wish it helps you!

If you still have questions about it, please kindly let me know!

Best Regards,

Kerry

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-----------------------------------------------------------------------------

0 件の賞賛
返信
2,755件の閲覧回数
dvdsosa
Contributor II

Hello Kerry,

I'm sorry, but with your answer, I still have the doubt.

Given that TTL is 5V (it is not the same as 3.3V), then, at which voltage works the UART from the FRDM-KW41Z? 5V or 3.3V?

Regards,

David.

0 件の賞賛
返信
2,753件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi david_sosa,

  KW41 is 3.3V.

  As I know, some TTL-USB tool can select 3.3V, this is an example:

 

image.png

 

Wish it helps you!

Best Regards,

Kerry

0 件の賞賛
返信