FRDM-KW 36 CAN Module issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KW 36 CAN Module issue

1,752件の閲覧回数
vardhan
Contributor I

In FRDM-KW 36 board I downloaded the SDK file from example projects(CAN loop back example code).I run the above example on MCU XPRESSO IDE, while debugging I am unable to read the data on CAN Pins(it means in CAN_H ,CAN_L & Transmit ,receive pins).

ラベル(1)
0 件の賞賛
返信
1 返信

1,737件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. In the readme.txt of the example you can see that "the example will send a CAN Message from the Tx Message Buffer to the Rx Message Buffer throuth internal loopback interconnect". The example shows how to use the loopback test mode to debug the CAN Bus design.

Can you check the flexcan_interrupt_transfer example? In this example, 2 boards are connected through CAN bus. You can find the Board settings in the readme.txt. And don't forget the 12V power supply on J32.

 

Best Regards,

Ricardo

0 件の賞賛
返信