External flash memory JN517x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External flash memory JN517x

2,434件の閲覧回数
jurijhuebner
Contributor I

Hi,

I am searching for a code example of an external flash memory.

BTW: Is it possible to use an flash memory which is not listed in  "JN51xx Boot Loader Operation"  document?

pastedImage_1.jpg

Regards,

J.

タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,280件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Jurij,

You can find some SPI Sample codes following this path.

C:\NXP\bstudio_nxp\sdk\JN-SW-4170\Platform\DK4\Source\LcdDriver.c

C:\NXP\bstudio_nxp\sdk\*SDK NUMBER*\Platform\DK4\Source\LcdDriver.c

You can use another flash, but be sure that the flash support the SPI protocol and the voltages that de JN supports.

Best Regards,

Mario

2,280件の閲覧回数
jurijhuebner
Contributor I

Ok found it, thank you

0 件の賞賛
返信