EPID does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EPID does not work

1,976 Views
liuxiang
Contributor I

Hello everyone:
Ask you a question, I use the JN5168, ZPS configuration editor configured EPID 0XAA, as shown in Figure

EPID.png
But I print LOG, get the node's EPID as follows: EPID: 0x00158d000035e687, MAC_ADDR = 0X00158d000035e687
Why is not the EPID I set the 0XAA? I think the EPID settings do not work, why is this? Ask you about, thank you.

Labels (1)
0 Kudos
Reply
1 Reply

1,799 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Liu,

If the pre-set value is zero, the Co-ordinator will use its own IEEE/MAC address as the EPID.

Note that the application may over-ride the EPID value set by the ZPS Configuration Editor by calling ZPS_eAplAibSetApsUseExtendedPanId() before calling ZPS_eAplZdoStartStack().

Best Regards,

Mario

0 Kudos
Reply