EPID does not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EPID does not work

1,983件の閲覧回数
liuxiang
Contributor I

Hello everyone:
Ask you a question, I use the JN5168, ZPS configuration editor configured EPID 0XAA, as shown in Figure

EPID.png
But I print LOG, get the node's EPID as follows: EPID: 0x00158d000035e687, MAC_ADDR = 0X00158d000035e687
Why is not the EPID I set the 0XAA? I think the EPID settings do not work, why is this? Ask you about, thank you.

ラベル(1)
0 件の賞賛
返信
1 返信

1,806件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Liu,

If the pre-set value is zero, the Co-ordinator will use its own IEEE/MAC address as the EPID.

Note that the application may over-ride the EPID value set by the ZPS Configuration Editor by calling ZPS_eAplAibSetApsUseExtendedPanId() before calling ZPS_eAplZdoStartStack().

Best Regards,

Mario

0 件の賞賛
返信