Distance of JN5168-001-M00 Module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Distance of JN5168-001-M00 Module

4,914件の閲覧回数
dheerajsawant
Contributor V

Hello Sir, 

davidashraf‌ mario_castaneda‌ 

I did data transfer between 2 JN5168-001-M00. 

but stuck in distance measurement. 

What is distance this Module occupied. 

while i was testing its giving me only 7-8 Meter Max distance. 

is this actual distance? or hardware changes required?

please reply soon. 

Thank You for your Time!

7 返答(返信)

4,336件の閲覧回数
davidashraf
Contributor V

Hello dheerajsawant‌ 

have a look at this thread 
https://community.nxp.com/thread/460781 

Regards

4,336件の閲覧回数
dheerajsawant
Contributor V

Hello David, 

I am trying to send data from coordinator to Sleeping Device(SED). 

but i have done little bit.

but problem is that only one time its receiving at SED point. 

(* and after one time my program goes to "PUBLIC void vWakeCallBack(void);" this function and  show whatever i am sending to Coordinator.)

please guide me.

Waiting for your reply.

Regards, 

Dheeraj 

0 件の賞賛
返信

4,336件の閲覧回数
dheerajsawant
Contributor V

Hello Friends, 

davidashraf‌ , mario_castaneda‌

(need Your Help)

I am still waiting for this problem's solution. 

please reply as soon as possible.

Thank You

0 件の賞賛
返信

4,336件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Dheeraj,

Did you ask this question in another community post? 

Could you please confirm?

Regards,

Mario

0 件の賞賛
返信

4,336件の閲覧回数
dheerajsawant
Contributor V

Hie mario_castaneda‌, 

I didn't ask to any other community yet. 

but still looking to solve that issue.

Best Regards, 

Dheeraj Sawant

0 件の賞賛
返信

4,336件の閲覧回数
dheerajsawant
Contributor V

Hello David, 

Yes its little bit increase my antenna strength.

before it was 7-8 meter max now i can receive up to More than 15 meter. 

that's now enough for me. 

Thank you for your reply

0 件の賞賛
返信

4,336件の閲覧回数
dheerajsawant
Contributor V

Hello David, 
Thank You for your Reply.

i will go through it.

I have another questions also

1) what its actual Range for data Transfer? because i think we cannot connect external Antenna to JN5168-001-M00

in PDF of JN5168-001-M00 they have written, we can connect Antenna only to JN5168-001-M03/05/06.

2) I want to send data transfer from Coordinator to Sleeping Device  


please reply me asap!

Thank You for Your Time!

0 件の賞賛
返信