Dhcp internet connection problem via ethernet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dhcp internet connection problem via ethernet

1,379件の閲覧回数
hkhunkim
Contributor I

When I boot, I have got below results

Configuring network interfaces... fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
eth0: adding address fe80::204:9fff:fe04:a712
eth0: waiting for carrier
fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
eth0: carrier acquired
DUID 00:01:00:01:22:ec:83:f3:00:04:9f:04:a7:12
eth0: IAID 9f:04:a7:12
eth0: probing address 192.168.0.10/24
eth0: soliciting an IPv6 router
eth0: using static address 192.168.0.10/24
eth0: adding route to 192.168.0.0/24
eth0: adding default route via 192.168.0.1
forked to background, child pid 403
done.

Even I change dhcpcd.conf or interface ip configuration, it always goes to 192.168.0.1 default route.

Can anyone suggest me what do I have to do?

ラベル(2)
0 件の賞賛
返信
1 返信

1,152件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

What part are you using ? 

Regards, 

Estephania 

0 件の賞賛
返信