Device automatically leaves the network

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Device automatically leaves the network

1,450 Views
yuboli
Contributor II

Hi, all;

I have some problems. Why does the device leave the network automatically sometimes when it enters the network

How can I avoid this problem?

Here is my packet capture log

0 Kudos
Reply
1 Reply

1,374 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Daniel, I hope you're doing well!

 

Are you using KW41Z? If so, could you please take a look at this community post here?

The sniffer log you provided and the one discussed there look very similar, so the problem could be related to the same issue.

 

Like the answer in the post describes, the issue could be related to the Link Key not being erased for the device, and the device not being able to decrypt the Transport Key command. If the command is instead sent with the default trust center link key, then it will be able to decrypt the transport key command.

 

Please let me know if the fix described in the answer doesn't work for you.

 

Best regards,

Sebastian

0 Kudos
Reply