Custom Board Support BeeStack #else /* gTarget_UserDefined_d */ no MCU_MKW24D512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Custom Board Support BeeStack #else /* gTarget_UserDefined_d */ no MCU_MKW24D512

1,411 Views
atillametetured
Contributor V

Hello,

I am trying to figure out the beestack port configurations. I have a custom board so gTarget_UserDefined_d should be 1.

In this case the macros include some headers given the MCU defined however even though there are tons of boards only a few MCU's in the PortConfig.h. Is this because other MCUs are covered by the boards? What should I do where I have a custom board that I want to adjust the port control registers of?

And also what is the explanation of that the code was generated with gTarget_UserDefined_d = 0 even though I selected custom target and MKW24D512 MCU during BeeKit?

Regards,

Mete

0 Kudos
Reply
0 Replies