Credit-based application with KW4x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Credit-based application with KW4x

2,119件の閲覧回数
koonlee
Contributor I

Hi,

I am referring to ipv6_router and ipv6_node examples from KW40/41Z connectivity software.

I understand it uses credit to control the amount of packets that can be sent. By default, the credit is 5 and after sending 5 packets, the sender needs to wait in order to obtain new credit to send again.

Would it be possible to increase the initial credit from 5 to, say 100? I try to change mAppLeCbInitialCredits_c to 50 in both ipv6_router and ipv6_node examples but it doesn't seem to work properly.

Thanks for your help!

タグ(3)
0 件の賞賛
返信
1 返信

1,939件の閲覧回数
alexandruandree
NXP Employee
NXP Employee

Hi,

You can change the number of credits like you said and the behavior will remain the same. Can you detail what do you see wrong and also on what software version are you testing?

BR,

Alex

0 件の賞賛
返信