Commissioning Thread sensors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Commissioning Thread sensors

3,159件の閲覧回数
sensenthuran
Contributor IV

Q1.

If we have different Thread sensors from various vendors, What are the minimal parameters need to be configured at commissioner for joining?

  1. Thread Short Eui / Long EUI / All FFF... &
  2. Pskd

Q2.

How we can set all the sensors with the corresponding PSKd to join an existing Thread nwk? Or is there any other easy way to commission? jcpacheco‌

Thanks

ラベル(2)
タグ(3)
3 返答(返信)

2,867件の閲覧回数
hung
Contributor II

Hello,

  How we can find nxp kw41z PSK and Long EUI address?

Thanks,

0 件の賞賛
返信

2,867件の閲覧回数
sensenthuran
Contributor IV

If you have kw41z loaded with thread router binary, in the shell command you can find..

$ thr get pskd
pskd: THREAD
 

$ thr get eui
eui: 0x0060376D0CCA9C5A

2,867件の閲覧回数
AleGuzman
NXP Employee
NXP Employee

Q1. The commissioner needs to know the joiner (sensor) PSKd and Long EUI Address through an out of band mechanisms like scanning a QR Code, user input, keypad etc..

Q2. Threadgroup recommends printing the PSKd and EUI at the end device package i.e. A QR Label may be scanned by a smartphone capable to communicate with a thread border router. Once the joiner credentials are known by a smartphone this can be used as the active commissioner.