Cannot capture packets through Ubiqua

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot capture packets through Ubiqua

2,529件の閲覧回数
yuboli
Contributor II

Hello,I have a JN5169USBdongle bought on the official website, I can use it to capture the package;

I have 5169 modules, so I want to make a few JN5169dongle, I burned the JN-SW-4168's own JefficSniffer firmware into the JN5169 module.

1552633536(1).png

Why can't I use Ubiqua to perform packet capture analysis on ZigBee?

1552632979(1).png

The application you selected is not supported by the firmware running on this devece,  why ?

Any one can help ? 
Thanks in advance .

0 件の賞賛
返信
3 返答(返信)

2,406件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Daniel,

Could you please try to program the JN devices using the next path?

C:\NXP\bstudio_nxp\sdk\JN-SW-4168\Tools\JennicSniffer\JennicSniffer_JN5169_1000000.bin

B. Installing a Packet Sniffer

Regards,

Mario

0 件の賞賛
返信

2,406件の閲覧回数
yuboli
Contributor II

Thank you!

I downloaded it according to your path, but I still can't.

pastedImage_1.png

pastedImage_2.png

My JN5169 module,as shown below

pastedImage_3.png

What is the reason for this?

0 件の賞賛
返信

2,406件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Daniel,

When you program the JN5169, you are in programming mode, the DO0 is in high, isn't it?

After that, the DO0 should be floating before the reset, with this the program will jump to the sniffer code.

Regards,

Mario

0 件の賞賛
返信