Can JN5189HN operate Zigbee and Thread simultaneously?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can JN5189HN operate Zigbee and Thread simultaneously?

跳至解决方案
2,601 次查看
andy_kim
Contributor IV

Hello, Community

I'd like to know if JN5189HN can operate Zigbee and Thread simultaneously like WiFi/BT combo module.

If it is available, where can I find the information about it?

 

Thank you.

 

Best regards,

Andy

标记 (1)
0 项奖励
回复
1 解答
2,582 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

I apologize, but  in this case the way to use both stack would be based on the time sharing as there is only one radio in the device, while we do not have examples with Thread and ZigBee working together , you can check the available examples for the K32W for some hybrid examples with BLE and Thread that you can use a a base for the development of the example you are looking for. Still, please take into consideration the memory footprint of both stacks plus the application size.

Regards

在原帖中查看解决方案

2 回复数
2,558 次查看
andy_kim
Contributor IV

Dear Estephania,

Thanks for your reply.

 

Best regards,

Andy

 

0 项奖励
回复
2,583 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

I apologize, but  in this case the way to use both stack would be based on the time sharing as there is only one radio in the device, while we do not have examples with Thread and ZigBee working together , you can check the available examples for the K32W for some hybrid examples with BLE and Thread that you can use a a base for the development of the example you are looking for. Still, please take into consideration the memory footprint of both stacks plus the application size.

Regards