Can Both bare metal and RTOS Run on MKW36A series SoC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can Both bare metal and RTOS Run on MKW36A series SoC

1,330 次查看
amalbabu
Contributor I

hi,

 We have considered MKW36/35A in on of our application. Can both Bare metal and RTOS run on MKW36A/35/34.

Is there any already developed RTOS which we can use for our application.

标签 (3)
0 项奖励
回复
1 回复

1,270 次查看
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Amal, I hope you're doing well!

 

If the application being developed is going to make use of the NXP BLE Stack, then some kind of RTOS will need to be implemented alongside the application. There are some existent RTOS that are already compatible with the KW36 family of MCUs, like Amazon FreeRTOS, or the custom built OS Abstraction component of the Wireless Connectivity Framework included with the Connectivity Stack.

This need for an RTOS is because the BLE stack needs to comply with the timing standards set by the BLE Specification, and the OS helps manage these timing requirements.

 

More information about these options can be read in the following documents:

<…\SDK_2.2.2_FRDM-KW36 - MCUXpresso\docs\rtos\Getting Started with MCUXpresso SDK and FreeRTOS OS.pdf>

<…\SDK_2.2.2_FRDM-KW36 - MCUXpresso\docs\wireless\Common\Connectivity Framework Reference Manual.pdf>

 

The SDK for the KW36Z can be downloaded from the MCUXpresso SDK Builder Website.

Please let me know if you need any more information.

 

Best regards,

Sebastian

0 项奖励
回复